What is the Endura WS5070?

Issue

What is the Endura WS5070?

Product Line

Pelco Video Management

Environment

Endura WS5070- All versions

Cause

Information regarding the WS5070 is needed.

Resolution

The Endura workstation WS5070 is a high-end personal computer running Windows Vista Business edition that is optimized for the WS5000 advanced system management software. The WS5000 advanced system management software is pre-installed and provides access to all of Endura’s operation and configuration features in one unified, user-friendly interface.