Issue
Can I program the buttons on the KBD5000?
Product Line
Pelco Video Management
Environment
Endura KBD5000- All versions
Cause
Information on the customizability of the KBD5000 is needed.
Resolution
No, the KBD5000 buttons are not customizable.