What is the network connection type on the WS5070?

Issue

What is the network connection type on the WS5070?

Product Line

Pelco Video Management

Environment

Endura WS5070- All versions

Cause

Information regarding the network connection on the WS5070 is needed.

Resolution

The WS5070 has one 10/100/1000Base-T Network Interface Card installed. In order to ensure proper performance, the WS5070 must be connected to a 1000Mbit/1Gb connection.