What is the maximum number of IP cameras supported by the DS1000?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

What is the maximum number of IP cameras supported by the DS1000?

Product Line

Pelco Video Management

Environment

DS1000

Cause

Install IP cameras based on the total number of IP cameras supported by the DS1000 series.

Resolution

The maximum number of IP cameras supported by DS1000 models are as follows:

  • DS 1000-F16 supports up to 16 IP cameras
  • DS 1000-F32 supports up to 8 IP cameras