What is the maximum number of streams that the DX8100 Series HVR supports?

Issue

What is the maximum number of streams that the DX8100 Series HVR supports?

Product Line

Pelco Video Management

Environment

  • DX8100 Series HVR

Cause

What is the maximum number of cameras that the DX8100 supports?

Resolution

The DX8100 Series HVR will support Analog and Pelco/Axis IP cameras.
Note: The total number of IP cameras depends on analog and IP camera settings and DX8100 system resources. You can record the maximum number of analog and IP cameras when all cameras are set to record at CIF/1 ips.

Model Maximum Analog Cameras Maximum Analog and IP Cameras
DX8108 8 24
DX8116 16 32
DX8124 24 32
DX8132 32 32

For more information on adding and analog or IP camera, refer to article: How do I setup analog and IP cameras in DX8100 Series hybrid video recorders?