How many streams can be displayed per NET5301R decoder?

Issue

How many streams can be displayed per NET5301R decoder?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

Endura NET5301R- All versions

Cause

Information regarding video stream capabilities for the NET5301R is needed.

Resolution

Simultaneously view up to four video streams on Composite Video, S Video, or VGA Monitor. When multiple streams are displayed, the video display frame rates adjust automatically to provide the best rate for the most recently selected camera.