UC, MR, and ASC controllers do not use the minimum trip and close command

Issue

Which controllers do not use the minimum trip and close command?

Product Line

TAC I/NET

Environment

UC, MR, or ASC

Cause

The editor lets you enter a value in the minimum trip and close field; however, the UCI, MRI, MCI, or I/Site Lan replaces the entered value with the default value of "0" when it is downloaded to the UC, MR, or ASC.

Resolution

The minimum trip and close parameters are not used for Unitary Controllers (UC), Micro Regulator (MR), or Application Specific Controllers (ASC) output commands.