Can the DS Quicksetup be installed as a stand alone software on the DigitalSentry NVS?

Issue

Can the DS Quicksetup be installed as a stand alone software on the DigitalSentry NVS?

Product Line

Pelco Video Management

Environment

  • Digital Sentry
  • DS NVs
  • DS Quick Setup

Cause

DS Quick Setup does not have a stand along installer and is part of the full Digital Sentry software install.

Resolution

No, you will need to go through a complete "Recording and Viewing Software" installation in order to get DS Quicksetup installed.