How can I configure the SEB5100 unit locally?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How can I configure the SEB5100 unit locally?

Product Line

Pelco Video Management

Environment

Endura SEB5100- All versions

Cause

Information on how to configure the SEB5100 is needed.

Resolution

The SEB5100 cannot be configured locally as there is no web interface. The NVR5000 automatically detects and configures the SEB5100(s). If you are having problems getting the SEB5100 to mount to the NVR/DVR, please see Lessons Learned Article #11533.