How do I display live video in a full screen view on the DX8100?

Issue

How do I display live video in a full screen view on the DX8100?

Product Line

Pelco Video Management

Environment

DX8100 Hybrid Video Recorder (HVR)

Cause

Expand the application window to occupy the entire monitor screen.

Resolution

  1. Select the live video mode.
  2. Select a window division.
  3. On the DX8100 toolbar, click the Full Screen  button. Live video is displayed in full screen view.

Click the right mouse button in the DX8100 window to display the DX8100 main window or exit full-screen from the full screen view