Playback video in full screen view on the DX8100.

Issue

How to playback video in full screen view on the DX8100.

Product Line

Pelco Video Management

Environment

DX8100 Series.

Cause

Increase area of view for video search.

Resolution

To display playback video in full screen view:
1. Select the playback mode.
2. Select a window division.
3. Left Click on desired camera and drag over and drop on screen
4. On the DX8100 toolbar, click the Full Screen button. Playback video is displayed in full screen view.

To display the DX8100 main window from the full screen view:
• Right click in the DX8100 window.