Is Endura Mapping 2.0 compatible with the EnduraXpress EE500 network video recorder?

Issue

Is Endura Mapping 2.0 compatible with the EnduraXpress EE500 network video recorder?

Product Line

Pelco Video Management

Environment

  • Endura EE500- Version 1.1.0.0051 +
  • Endura WS5000- Version 2.3.0-9084 +
  • Endura Mapping- 2.2.0-4817 +

Cause

Information on the compatibility of the EE500 and the Endura Mapping software is needed.

Resolution

Yes. The software version for each product must be running the following version or higher:
 
Product Software Version
EE500 01.01.00.0051
Endura Mapping System Installer 2.2.0-4817
Endura Mapping 2.2.0-4817
WS5000 2.3.0-9084