Which Sarix IP cameras have the capability or need to use 24VAC?

Issue

Which Sarix IP cameras have the capability or need to use 24VAC?

Product Line

Pelco Cameras, Pelco Transmission & Power

Environment

When using the Sarix line of cameras

Cause

When to  use 24 VAC for power, mostly seen when using heaters

Resolution

The Sarix cameras that can use 24 VAC are usually outdoor units that use heaters, the exception to this is the IM series which is strictly PoE.

The  IX, IXE, ID, IEE, IE, IDE, Spectra IV, Exsite, and Esprit can use 24 VAC and in some cases require it 

Sarix IXES1, IXE11, and IXE31 models are PoE only.