What is the Ethernet connection type on the SEB5100?

Issue

What is the Ethernet connection type on the SEB5100?

Product Line

Pelco Video Management

Environment

Endura SEB5100- All versions

Cause

Information on the ethernet ports on the SEB5100 is needed.

Resolution

The SEB5100 has two Gigabit Ethernet RJ-45 ports (1000Base-T).