How do I identify the Endura SEB5100 storage expansion box software version?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do I identify the Endura SEB5100 storage expansion box software version?

Product Line

Pelco Video Management

Environment

Endura SEB5100- All versions

Cause

Information on how to determine the version of software on the SEB5100 is needed.

Resolution

The SEB5100 software version is not exposed in the user interface. Typically the software version of the SEB5100 is the same as network video recorder (NVR) or digital video recorder (DVR).  

To determine the version number either SSH into the SEB from the NVR/DVR or attach a monitor and keyboard directly to the unit. For the procedure on how to locate and login to a SEB5100 using SSH please see Lessons Learned Article #10873.

  1. From the command prompt on the SEB5100, enter cd /usr/local/Pelco/NSD/Public
  2. Then enter more Manifest.xml
  3. The software version will be displayed between the "packageversion" tags.