Why am I unable to make any SETUP MENU changes for the Camclosure 2?

Issue

Why am I unable to make any SETUP MENU changes for the Camclosure 2?

Product Line

Pelco Cameras

Environment

  • IS20
  • IS50

Cause

Menu is not allowing to enable.

Resolution

If the setup menu is called up with the operation buttons while a camera image is displayed, the setup mode is always "DISABLE" to prevent operation errors.

  1. Press the up or down button to move the cursor to the "END".
  2. Press the right button to move the cursor to "SETUP," and press the "SETTINGS" button to change the setup mode from "DISABLE" to "ENABLE."
  3. The setup mode changes to "ENABLE," and the Setup menu is ready to be set.