Camclosure 2 displays the text DISABLE when trying to access camera menu

Issue

Why does Camclosure 2 display the text DISABLE when trying to access camera menu?

Product Line

Pelco Cameras

Environment

  • IS20/21
  • IS50/51

Cause

Accessing of menu for Camclosure 2

Resolution

If the top screen of the setup menu is called up with the operation buttons while a camera image is displayed, the setup mode is always "DISABLE" to prevent operation errors.

To access Setup Menu:

  1. Hold down the setting button for more than 2 seconds simultaneously to call up the top screen of the setup menu.
  2. Press the up or down button to move the cursor to "END".
  3. Press the right button to move the cursor to the "SETUP," and press the setting button to change setup mode from "DISABLE" to "ENABLE," and the Setup menu is ready to be set.