What are the maximum number of cameras on one CM9700 Noded System?

Issue

What are the maximum number of cameras on one CM9700 Noded System?

Product Line

Pelco Matrix

Environment

CM9700 Noded System

Cause

Total number of cameras supported on one node.

Resolution

On a CM9765 and CM9770, the maximum number of cameras per node is 2,048 cameras.
On a CM9870, the maximum number of cameras per node are 4,096 cameras.