What is I-VMD feature for the Super Dynamic 5 (SD5) camera?

Issue

What is I-VMD feature for the Super Dynamic 5 (SD5) camera?

Product Line

Pelco Cameras

Environment

SD5 camera

Cause

Product feature specification.

Resolution

The I-VMD feature is an intelligent built-in video motion detector that provides more efficient and reliable surveillance, while eliminating the loss of notification in vital scenes. Using advanced motion analytics provides the ability to accurately detect motion within a targeted area. The I-VMD analytics include three behaviors: Motion Detection, Object Abandonment/Removal, and Scene Change Detection.