How to start or stop an automatic cycle view mode in the DX8100

Issue

How to start or stop an automatic cycle view mode in the DX8100

Product Line

Pelco Video Management

Environment

DX8100 Series recorder

Cause

Turns window cycling on and off. Automatically cycles through each view panel ensuring all cameras get displayed.

Resolution

To turn ON/OFF the automatic cycle view mode:

  • To start the automatic cycle view mode on the DX8100, click the Cycle Views  button on the DX8100 toolbar.
    Note: The Cycle Views icon turns blue, indicating that the DX8100 is in the automatic cycle view mode. The system will cycle through each panel, displaying each panel for the configured cycle view dwell time.
     
  • To stop the automatic cycle view mode on the DX8100, click the Cycle Views  button on the DX8100 toolbar.