How do I control which groups can modify the cycle view dwell time on the DX8100?

Issue

How do I control which groups can modify the cycle view dwell time on the DX8100?

Product Line

Pelco Video Management

Environment

DX8100 Series hybrid video recorder (HVRs)

Cause

Set permission to modify the cycle view dwell time.

Resolution

The DX8100 allows the Administrator to control which user group can change the cycle view dwell time. In this case, anyone that belongs to a selected user group can change the cycle view dwell time.
 
To select a user group to have permission to change the cycle view dwell time:
1. On the DX8100 toolbar, click the Live button.
2. From the DX8100 menu bar, choose View > Cycle Views Setup > Dwell time change.
3. From the Dwell time change submenu, choose a user group.