How do I manually cycle through hidden view panels on the DX8100?

Issue

How do I manually cycle through hidden view panels on the DX8100?

Product Line

Pelco Video Management

Environment

DX8100 Series hybrid video recorder (HVRs)

Cause

The 36-division display format was not selected, which the DX8100 displays the panes in multiple panels and must cycle through multiple panels to display hidden channels.

Resolution

To manually cycle through hidden view panels:
  1. On the DX8100 toolbar; click one of the panel division buttons. The view sequences through the view panels.
    For example, when you repeatedly click a 4 Division display format button, the DX8100 cycles through each of the eight available panels.