Is the ICS110-BV breather vent needed in addition to the ICS110-PG pendant mount adapter?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Is the ICS110-BV breather vent needed in addition to the ICS110-PG pendant mount adapter?

Product Line

Pelco Cameras

Environment

  • IS110 Models
  • ICS110 Models

Cause

Breather Vent application

Resolution

Yes, if the weather at location has a high amount of rain/humidity.

View the ICS110-BV manual here.