What is the NVR5000?

Issue

What is the NVR5000?

Product Line

Pelco Video Management

Environment

NVR5000

Cause

Information of NVR500 Series recorders

Resolution

The NVR5000 Series is the network video recorder capable of continuous, schedule, alarm/event, and motion recording. Pre- and post-alarm, event, and motion recording is also available and is fully programmable on a per-channel basis. An advanced and unique feature is built into the NVR5000 for maximizing storage efficiency by removing unwanted data using a time- and priority-based system.