Does the SD427-PG-E1 and DS NVR do coaxitron control for the PTZ?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Does the SD427-PG-E1 and DS NVR do coaxitron control for the PTZ?

Product Line

Pelco Cameras

Environment

  • Spectra IV (analog)

Cause

PTZ control options of camera

Resolution

The NVR does not have analog inputs so the Spectra IV would need to have an IP converter to work in extended coaxitron mode.