Total number of RS-422 ports on the CM9700 Matrix Systems

Issue

  • How many data ports are available on the CM9700 Matrix Systems?
  • How many Data Ports can I have on my CM9700 Series Matrix Switcher?

Product Line

Pelco Matrix

Environment

CM9700 Matrix System

Cause

Expand data ports to provide communication with external devices.

Resolution

The CM9700 Matrix Series System comes from the factory with sixteen data ports and two RS-232 Ports. The CM9700 Series System can be expanded up to 120 data ports (Sercom) by adding three CM9700-SER-32 port expansion units (32 ports each) to the CC1.