Is a 24 hour export possible on the DX8100?

Issue

Is a 24 hour export possible on the DX8100?

Product Line

Pelco Video Management

Environment

DX8100 Series

Cause

When using the export feature users can't bookmark past a day.

Resolution

No. Only export 22 hours, if need to do more hours, then use the backup feature to backup to a network drive or USB storage device.