My Camclosure 2 is displaying the text of OVER HEAT. What does this mean?

Issue

My Camclosure 2 is displaying the text of OVER HEAT. What does this mean?

Product Line

Pelco Cameras

Environment

  • Camclosure 2
  • IS50/IS51

Cause

Video displaying message of OVER HEAT

Resolution

The OVER HEAT message displays when environmental conditions exceed the cameras operating conditions. Avoid installing this product in locations where the temperature is not within -10°C to 50°C (14°F to 122°F). When using the heater unit, the product can be used within -30°C to 50°C (-22°F to 122°F) and humidity below 90%.