Connect a KBD300A or Digital Video Recorder to a Spectra IV IP camera using RS422 2-Wire control.

Issue

How to wire the RS422 connections of a control device such as the KBD300A or Digital Video Recorder to a Spectra IV IP camera?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Spectra IV IP TXB-N
  • Spectra IV IP TXB-IP
  • Digital Video Recorder
    • DSSRV using ENC5416
    • DX4700/4800(HD)
    • DX8100
    • DX4500/DX4600
  • KBD300A

Cause

Pan/Tilt/Zoom function using RS422 2-Wire control.

Resolution

From the controller device, wire the TX+/TX- terminals to the cameras Rx+/Rx- as you would a standard analog Spectra IV.

Note: TXB-N only supports Pelco D protocol at 2400 baud. By default the TXB-N is set to Pelco D address 1, if the address needs to be changed you will have to reset the TXB-N board.

Note: The TXB-IP will allow for Pelco D or Pelco P at 4800 baud.

Related Articles:

Reset Spectra IV IP and h.264 series encoder board.