What are the zoom limits on the Spectra IV series camera?

Issue

What are the zoom limits on the Spectra IV series camera?

Product Line

Pelco Cameras

Environment

Spectra IV series

Cause

Spectra IV zoom options.

Resolution

There are 3 models of the Spectra IV series each with different lens options.

  • 36X at f/1.4 (focal length, 3.3-119 mm)
  • 29X at f/1.4 (focal length, 3.4-98.6 mm)
  • 23X at f/1.6 (focal length, 3.6-82.8 mm)