Is there a way to see the same alarms we get on the Endura Workstation, on the Video Console Display (VCD)?

Issue

Is there a way to see the same alarms we get on the Endura Workstation, on the Video Console Display (VCD)?

Product Line

Pelco Video Management

Environment

  • Endura WS5000/WS5200- All versions
  • Endura VCD5000/VCD5202- All versions

Cause

Information on how to receive alarms on the VCD is needed.

Resolution

  • Also see Related Lessons Learned Article LL#12273

Important Note: When changing user roles the WS5000 and VCD5202 users will be required to log out then log back in to take affect.

Yes.  If the operator has subscribed to receive alarm messages, alarm messages will be displayed to the Workstation and the Video Console Display. Operators may subscribe to these alarm messages from the WS5000 software, under Setup> Users> Alarm Notification.