What is a WS5200-1?

Issue

What is a WS5200-1?

Product Line

Pelco Video Management

Environment

  • Endura WS5200-xx - All versions
  • Customer Supplied PC

Cause

Information on the product number WS5200-1 is needed.

Resolution

The WS5200-1 is a software solution that is installed on a customer supplied PC.  The WS5200-1 part number is a physically shipped software disk.  This is a single license seat for 1 PC.  For additional license offers and information on the WS5200 software including PC requirements, please see the spec sheet.  

REGISTERING THE APPLICATION: Click here: WS5200