NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
What storage expansion options are available for the DX4500/DX4600 server?
Product Line
Pelco Video Management
Environment
- DX4500 Series
- DX4600 Series
Cause
Want to add more storage space to the DX4500/DX4600.
Resolution
To following hard drive upgrade kits are available to increase storage.
Part Number | Description |
DX4546HDD250KIT | DX4500/DX4600 SATA 250 GB upgrade |
DX4546HDD500KIT | DX4500/DX4600 SATA 500 GB upgrade |
DX4546HDD750KIT | DX4500/DX4600 SATA 750 GB upgrade |
DX4546HD1000KIT | DX4500/DX4600 SATA 1000 GB upgrade |
DX4546HD2000KIT | DX4500/DX4600 SATA 2000 GB upgrade |
Note: The DX4500 supports a maximum storage capacity of 4 Terabyte (TB). 2 drives.
The DX4600 supports a maximum storage capacity of 8 Terabyte (TB). 4 drives.
NOTE: These kits are now all obsolete. Please call in to sales for current part numbers for replacement and upgrade hard drive part numbers and availability.
Related articles: