Is Endura compatible with existing Pelco products?

Issue

Is Endura compatible with existing Pelco products?

Product Line

Pelco Video Management

Environment

Endura system- All versions

Cause

Information regarding compatibility of the Endura system and existing Pelco products is needed.

Resolution

Yes, any analog camera can be introduced into an Endura environment via the use of an Endura Encoder. Additionally, the Endura system has the capability of integrating with a CM9700 Matrix system via the UDI5000-MTRX.