Is Spectra IV IP compatible with Microsoft Internet Explorer 8.0 (IE8) or Mozilla Firefox 3.6?

Issue

Is Spectra IV compatible with Microsoft Internet Explorer 8.0 (IE8) or Mozilla Firefox 3.6?

Product Line

Pelco Cameras

Environment

  • Spectra IV IP Series

Cause

Viewing and PTZ support of Spectra IV IP through browser

Resolution

Yes. You can control the Spectra IV with IE8 or Firefox if the unit has a TXB-IP or TXB-N module.