What is a preset?

Issue

What is the definition of a Preset location that used on the Spectra IV or Esprit systems?

Product Line

Pelco Cameras

Environment

  • Spectra Models
  • Esprit Models
  • ExSite Models

Cause

Definition of preset

Resolution

A preset is a script that allows users to a save a camera's position, zoom, and other settings such as auto-iris and auto-focus; collectively as a 'bookmark'. Users can save multiple presets per camera. For example if a user monitoring several specific points using the same camera, the user can set one preset for the main entrance with a moderate zoom value, and the user can set another preset for a vulnerable window, lying some ways from the main entrance, with a higher value zoom value and a specific position.