How to change the Date and Time of a Genex Multiplexer

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do I change the date and time on a Genex using the KBD4000 or Genex Multiplexer front panel controls?

Product Line

Pelco Matrix

Environment

  • MX4016CD
  • MX4009CD
  • KBD4000

Cause

Setting Time and Date of Genex

Resolution

The time and date of the genex series multiplexer can be changed by either of two methods:
 

FRONT PANEL: To change from Genex front panel

  1. Hold down the VIEW button until the SYSTEM SETUP menu displays.
    PASSWORD: See article "Genex Series Password" here
  2. Use the Directional Arrows to move the edit bar over the TIME field.
  3. Use the +/- button to change to the correct time.
  4. Move the edit bar to EXIT.
  5. Press the +/- button to EXIT.  

 


 

KBD4000: To change from the KBD4000 keyboard

  1. Hold down the VIEW button until the SYSTEM SETUP menu displays.
    PASSWORD: See article "Genex Series Password" here
  2. Use the Joystick to move the edit bar over the TIME field.
  3. Use the OPEN/CLOSE buttons to change to the correct time.
  4. Move the edit bar to EXIT.
  5. Press the OPEN/CLOSE button to EXIT.

    Note: Switch 8 on the KBD4000 must be ON (down position) for programming of Genex

       

 

Related Lessons Learned Articles:
Genex Series Password
How to turn off time display of the Genex