How do I manually set the PTZ baud rate in the Endura WS5000 Advanced System Management Software?

Issue

How do I manually set the PTZ baud rate in the Endura WS5000 Advanced System Management Software?

Product Line

Pelco Video Management

Environment

Endura WS5000- All versions

Cause

Information on how to set the baud rate from the WS5000 software is needed.

Resolution

To adjust the PTZ baud rate setting:

  1. Click on Setup
  2. Under the Devices tab, click on the Filter icon in the top left corner.
  3.  Adjust Filter Types to show Device Type.
  4. Adjust Device Type to show Encoder
  5. Adjust the Serial Port Settings to match the camera