How do I access the Spectra or Esprit camera menu using KBD300A with CM6800 Matrix?

Issue

How do I access the Spectra Dome menu through the CM6800 Matrix Switcher

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM6800 Matrix Switcher (All Version)
  • KBD300A keyboard (All Version)
  • KBD200A Keyboard (All Version)
  • Spectra
  • Esprit
  • ExSite
  • Spectra Mini

Cause

Access Spectra Dome to configure settings.

Resolution

  1. Enter 95
  2. Hold PRESET for 2 seconds.
  3. Preset Label menu will appear on monitor.
  4. Move down to the SET and it will start flashing.
  5. Move joystick to right or press right button 
  6. Camera menu will open.

See Lessons Learned Article #11203 for other systems access camera menu.