Bi-directional audio capability on the DX4700/DX4800 Series HVRs

Issue

Do all 16 channels have bi-directional audio capability on the DX4700/DX4800 Series HVRs?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series hybrid video recorder (HVRs)

Cause

Utilize more than one channel bi-directional audio at once. 

Resolution

Yes, but not simultaneously. The system has the capacity for one channel bi-directional audio at a time.

To hear live and playback audio at the server, connect a speaker to Audio Out 1.

To hear live audio received from the DX Series client, connect a speaker to Audio Out 2