What are the resolution options available for a camera on the DX4500/DX4600?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

What are the resolution options available for a camera on the DX4500/DX4600?

Product Line

Pelco Video Management

Environment

DX4500/DX4600 Series digital video recorder (DVR)

Cause

Configure camera settings.

Resolution

The DX4500/DX4600 can record at the following resolutions:
 

NTSC PAL
704 x 480 704 x 576
704 x 240 704 x 288
352 x 240 352 x 288