What is the maximum number of bookmarks the DX4500/DX4600/DX4700/DX4800 Series hybrid video recorder (HVRs) support?

Issue

What is the maximum number of bookmarks the DX4500/DX4600/DX4700/DX4800 Series hybrid video recorder (HVRs) support?

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600 Series HVR
  • DX4700/DX4800 Series HVR

Cause

Information on the total number of supported bookmark on the system, which is use to mark a video clip for Bookmark Search.

NOTE:  Bookmarks are ONLY used for searching video. A Bookmark cannot be exported.

Resolution

Total number of bookmark is 10