Is coaxitron protocol supported on the DX4700/DX4800 Series HVRs?

Issue

Is coaxitron protocol supported on the DX4700/DX4800 Series HVRs?

Product Line

Pelco Video Management

Environment

  • DX4700/DX4800(HD) all versions
  • Pelco C / Coaxitron PTZ protocol

Cause

For coaxitron control on the DX4700/DX4800 system, the protocol needs to be enabled.

Resolution

Yes. Coaxitron protocol is supported and needs to enable on the DX4700/DX4800 recorder.

Related articles:

Configure the DX4700, DX4800 HVR for Over the Coax or 2 wire PTZ control.