What are the KBD300A keyboard functions with the DX4700/DX4800 (HVRs)

Issue

Is the KBD300A keyboard compatible with the DX4700/DX4800 Series hybrid video recorders (HVRs)?

Product Line

Pelco Video Management, Pelco Matrix

Environment

  • KBD300A
  • KBD300USBKIT
  • DX4700 non HD (Version 1.02 and higher)
  • DX4800 non HD (Version 1.02 and higher)
  • DX4700(HD) (Version 2.0 and higher)
  • DX4800(HD) (Version 2.0 and higher)

Cause

Adding a KBD300A to a DX4700/4800

Resolution

Yes. However, a USB kit is required for connectivity. The part number is KBD300USBKIT.
Note: A user MUST be logged in to PTZ cameras, Guest user can change camera views only.
 
 
KeyBoard Function: Changing screen display
 
  1. On the KBD300A Press the Shift Button and the Green LED will turn On.


     
  2. Press the F2 button (single screen).


     
  3. Verify Main monitor switches to single screen displays.
     
  4. Press the 1 button then the CAM button. (Number + Cam) 


     
  5. Repeat steps four to call up a different camera display.
     

KeyBoard Function: Control PTZ

  1. Log into the DX4700/DX4800.(required for PTZ)
  2. On the the KBD300A press Shift button (LED on) to select the main monitor screen on the DX4700/DX4800.


     
  3. Press the F2/F3/AUX to change to one of the Multiple screen.


     
  4. Once screen is selected, Move the KBD300A Joy stick (up/down/left/right) until a white outer box is on the PTZ camera.


     
  5. Once the white outer box is on the PTZ camera press the Shift button (LED off)


     
  6. Move the the KBD300A joystick and the PTZ will follow.    

     

Related articles:
How to connect the KBD300USBKit with the DX4700/DX4800 series DVR.

Is the KBD300A keyboard compatible with the DX4700/DX4800 Series hybrid video recorders (HVRs) and what are it's functions.