Is a digital storage estimator available for the DX Series recorder?

Issue

Is a digital storage estimator available for the DX Series recorder?

Product Line

Pelco Video Management

Environment

  • DX4100
  • DX4500/DX4600
  • DX4700/DX4800
  • DX8100
  • Pelco Digital Storage Estimators

Cause

Help determine the amount of recording space required based on a number of variables.

Resolution

Yes. To download the current DX Storage Estimator, follow the instruction below:
  1. Go to the Tools and Calculators homepage.
  2. Under VMS Tools, Calculators & Mobile Apps section, click on the link  "Download the Digital Storage Estimator" to start downloading.