Is automated failover capability available on the DX4700/DX4800 Series hybrid video recorders (HVRs)?

Issue

Is automated failover capability available on the DX4700/DX4800 Series hybrid video recorders (HVRs)?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series HVRs

Cause

To have one DX4700/DX4800 system as the backup in case of the main DX4700/DX4800 system failed is not supported on the DX Product Line.

Resolution

There are no plans on a failover process at this time. The capability is available with the Endura products.