How many monitor outputs on the DX4700/DX4800 Series hybrid video recorders (HVRs)?

Issue

How many monitor outputs on the DX4700/DX4800 Series hybrid video recorders (HVRs)?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series HVR

Cause

Video output option on the DX4700/DX4800 series for additional monitoring.

Resolution

One main (either VGA or BNC) and one spot monitor on BNC - spot can be single camera or quad and either fixed cameras or pop-up on alarm. The spot monitor is for analog cameras only.