What is the difference between the DX4700 and DX4800 Series hybrid video recorders (HVRs)?

Issue

What is the difference between the DX4700 and DX4800 Series hybrid video recorders (HVRs)?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series HVRs

Cause

Seek information on the difference between the DX4700 and DX4800 series.

Resolution

Recording Standards

DX4800 series has higher recording standards than the DX4700 series as shown in the chart below:

Audio

  • DX4700 has two mono RCA line in audio inputs
  • DX4800 has four mono RCA line in audio inputs