What display modes are available on the DX4700/DX4800 Spot Monitor output?

Issue

What display modes are available on the DX4700/DX4800 Spot Monitor output?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series HVR

Cause

View layout options on the Spot output monitor provide additional monitoring option.

Resolution

There is one Spot Monitor output on the server that can be configured to display video from channel 1, 2, 3, or 4 in single or quad mode, including sequence video.

Note: The Spot Monitor cannot display video from IP cameras.