Is the Endura NET5400T Series encoders compatible with the DX4700/DX4800 Series hybrid video recorders?

Issue

Is the Endura NET5400T Series encoders compatible with the DX4700/4800 Series hybrid video recorders?

Product Line

Pelco Video Management

Environment

DX4700/DX4800 Series HVR
Endura NET5400T Series Encoder

Cause

Different platform.

Resolution

No, the Endura NET5400T Encoder is not compatible with the DX4700/DX4800 Series. To use the Endura NET5400T Encoder, the system need to be upgrade to DX4700HD/DX4800HD Series.